AXIS#.BODE.VAMP

Description

AXIS#.BODE.VAMP sets the amplitude of the excitation when in velocity mode as set in AXIS#.BODE.INJECTPOINT.

Example

Set the excitation velocity to 100 RPM:

--> AXIS1.BODE.VAMP 100

Get the excitation velocity (already set to 100 RPM):

--> AXIS1.BODE.VAMP
100.000 [rpm]

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

0 RPM

Depends on units. See Velocity Units for details.

Data Type

Float
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
AXIS1.BODE.VAMP

5001h

03h

Signed32

Velocity

-

Read/Write

No

AXIS2.BODE.VAMP

5101h

03h

Signed32

Velocity

-

Read/Write

No